Motor_Stall_Max_Err_Angle

Motor_Stall_Max_Err_Angle

Address: 8200 (2008H)
Type: UWORD
Access: Read/Write
Unit: 0.01 radian
Range: 0 to 65535
Default Value: 1256
Store Supported: Yes
Description: This object defines the maximum allowed displacement between theoretical angle and estimated angle of motor rotor position for ‘Motor Stall detection’ feature.  When the displacement limit is reached, the motor is stopped (Min_Current object value is applied to motor) and alarm is issued.
Notes:

See Motor Stall Detection for more details about ‘Motor Stall detection' feature.

This object is available only with firmware version V02r74 or superior.